The high costs of refrigeration equipment can be prohibitive for businesses, so it's crucial to explore all of the options available for acquiring the technology you need for your company. One opportunity businesses can use to save money is to shop for quality preowned refrigeration equipment. Preowned refrigeration equipment can be an excellent option for businesses on a tight budget, as it can be significantly cheaper than purchasing new equipment. Additionally, when you buy from a reliable retailer, you can trust that your equipment will function well and efficiently. Businesses can still get the performance they need without breaking the bank. If this sounds like something your business could use, keep reading to learn more on how to shop for pre-owned industrial refrigeration equipment.
How can you shop for preowned refrigeration equipment?
When shopping for preowned industrial refrigeration equipment, it's crucial to consider the size of the unit, the type of refrigerant it uses, and the voltage it needs. You should always compare prices and find the best deal. Refrigeration equipment is available from a variety of sources, including us here at Genemco. With over 30 years in the industry, Genemco is a name you can trust when it comes to finding the best quality industrial equipment. Refrigeration equipment is available in a range of sizes, so you should choose the best size for your space and needs. Most equipment also requires a specific voltage. Look for equipment that is compatible with your electrical system.
There are several refrigeration systems, but absorption, mechanical, and vapor compression are the most common types. Absorption systems use hydrogen gas and ammonia liquid to create a cooling effect. Mechanical systems use refrigerant gas to transfer heat from the cooled object to a condenser. Vapor compression systems are the most common type of refrigeration system. They use a compressor to increase the pressure of a refrigerant gas, which causes it to condense and release heat.
Once you've determined the right type of refrigeration system for your business, you need to decide which system is right for you. Split systems are another common choice. Some examples include a freon refrigerant compressor rack or a split system condensing unit with a remote air handler. These systems are composed of outdoor and indoor units and can minimize noise and better regulate the temperature. You also won't have to run ductwork through the entire space. The outdoor unit extracts heat from the air, and the indoor unit discharges the cooled air. You can also find packaged refrigeration units. These systems comprise a single unit containing the compressor and the condenser.
Capacity is another primary consideration. The capacity of a refrigeration system is measured in British thermal units (BTUs). You need to choose a system with a capacity that's appropriate for your business. Additionally, some refrigeration systems are more energy efficient than others. Because the industry is moving towards increased energy efficiency, newer preowned refrigeration equipment models may be your best bet to fit your budget.
What are some common types of refrigeration equipment you can purchase used?
Refrigeration equipment is necessary for businesses that store or transport food or other products at a specific temperature. Used industrial refrigeration equipment can include industrial refrigerators, IQF tunnels, ice makers, blast freezers, and chillers. These types of equipment may be required for businesses in the food service industry, the grocery industry, the pharmaceutical industry, and the manufacturing industry. They can also be used in other types of industrial settings, like food processing and beverage processing facilities. Let's review a few examples of industrial refrigeration equipment that businesses can purchase preowned.
Evaporator coils are a common piece of refrigeration equipment. They are used in many businesses, particularly within the food and beverage industry. Evaporator coils are an essential part of food and beverage manufacturing. They are used to remove excess water from the air, which helps to keep the manufacturing process running smoothly. Evaporator coils also help to keep the space and your products clean and free of moisture, which can help to prevent the growth of bacteria and other contaminants. Since they are built to last, you can safely purchase a preowned coil for your business.
Industrial freezers and walk-in coolers are also necessary for many food and beverage operations. A walk-in cooler is a refrigerated room or chamber used to store food or other perishables at a temperature below the ambient temperature. Walk-in coolers are typically used in restaurants, grocery stores, and other commercial food service operations. They are generally large enough to store several pallets of food and other items.
A cooling tower is another popular piece of industrial refrigeration equipment. It's used to remove heat from a liquid or gas. You can find high-quality used fiberglass cooling towers, which cool water through evaporative cooling. The water is pumped up to the top of the tower, where it flows over the surface of the many fiberglass panels. The water evaporates, cooling the water and the air around it. The cooled water then flows back down to the bottom of the tower and is recirculated.
What else can you do to protect your business's inventory?
Many items require some form of climate-controlled storage to provide low temperatures, even if they don't need to be frozen in an industrial freezer or a walk-in cooler. If you are wondering if you need climate-controlled storage, ask yourself if the items you plan to store will be affected by extreme changes in temperature. Temperature changes can cause materials to warp, rot, or mildew. Thorough training on how to use the industrial refrigeration your business relies on can help you avoid costly mistakes in the cooling process. When your employees know how to use and maintain the industrial refrigeration system, it will keep your business running smoothly and avoid costly breakdowns.
When it comes to purchasing equipment for refrigeration, there’s no question that you want the best for your business. However, sometimes that can be out of reach financially. That’s where preowned equipment comes in. If you are looking for to add or improve refrigeration for your business, preowned industrial refrigeration equipment can be a fantastic option. It offers similar performance as new equipment but at a fraction of the cost. Make sure that you are getting a quality product and that you are aware of the price of shipping and installation. If you follow this valuable advice, you can trust that your business can maintain an effective refrigeration process.