Gas Compressors
Shop for Industrial gas compressors from leading manufacturers.
Gas compressors are designed to process gases like natural gas, hydrogen, nitrogen, and air.
- FAQs
These compressors function by displacing gas and reducing its volume to increase pressure. There is a motor and a compressor station that performs the actual gas compression. The compressor station or unit contains several key components, such as cylinders, pistons, valves, belts, and a lubricant system.
The motor starts and spins a crankshaft. These power the movement of pistons inside the cylinders. The pistons move downward and a mixture of gas and air enters the cylinder through an intake valve. The piston moves back up and compresses gas inside the cylinder. This compression action reduces the volume of the gas and consequently results in higher pressure.
Some of the most common applications for these compressors include the oil and natural gas industry as well as the manufacturing industry. Both upstream and downstream operations use these types of compressors, as well as pneumatic operations and material handling. They can also be used for power generation as well as the petrochemical and aircraft industry. Overall, they have diverse applications throughout various industries.
The main difference between the two compressors is the type of fluid that they compress. Air compressors are specifically for air, while the gas type compresses natural gas, refrigerant gas, and other industrial gases. They store and transport these components differently. Air compressors are also generally simpler in design and construction.
- Several different types serve various purposes. Each one operates uniquely and has its own benefits. Check out some of the most common options below:
- Reciprocating compressor: These industrial gas compressors use a piston within a cylinder to compress gas. They're known for their high pressure-compression ratio.
- Rotary screw compressor: These units are characterized by two rotating metal screws that efficiently compress gas using friction.
- Rotary vane compressor: The rotary vane compressor has adjustable rotary vanes that push against a cylinder wall to compress gas.
- Centrifugal compressor: This type of compressor uses centrifugal force to create compression.
You can shop for industrial compressors or tools right here at Genemco. We sell equipment from the top brands and aim to help with energy efficiency and energy saving. Feel free to contact our customer service team for assistance with choosing industrial equipment.
Top Sellers
View all