Rotary Vane Compressors
Genemco sells used vane compressors to help with energy efficiency and energy saving.
We offer Used Rotary compressors from major brands.
- FAQs
Rotary vane compressors are a type of compressor unit that uses adjustable rotary vanes powered by an electric motor. The cylinder housing and the off-centered drive shaft allow the vane compressors to deliver high-quality compressed air consistently. The unit is energy-efficient and its design features a rotor with vanes that move in and out of the rotor chamber or valve to create compressed air.
Now that you know the answer to the question, "What are rotary compressors?" you may be interested in understanding how exactly they work. The compressor unit operates using rotating vanes inside the cylinder housing powered by an electric motor. The vanes are offset, which creates chambers with different volumes as they spin. The rotor inside spins and centrifugal force pushes the vanes out of a valve, forming a seal against the housing wall.
The seal creates compartments that trap gas, and the rotor continues to spin to create compressed air. This air is then discharged through an outlet value while fresh air is drawn in through an inlet valve. Then, the cycle repeats itself, generating compressed gas suitable for numerous manufacturing applications.
- There are many advantages to using rotary compressors, but vane compressors in particular. Here is a list of reasons why it may be a great option for manufacturing use:
- Durability: With proper maintenance and high-quality materials, rotary vane units can have a long lifespan. It can withstand heavy-duty operations and everyday wear in manufacturing facilities, and this ensures reliable performance and operational efficiency.
- Energy efficiency: Rotary vane units also utilize minimal energy. If your facility wants efficiency without overconsumption of energy, these compressors are a great tool without running up the cost of your utility bill.
- Low noise levels: Rotary compressors and machines deliver a consistent flow of air with low volume and vibration which makes them ideal for noise-sensitive environments.
Compact construction: Rotary vane units have a compact design or construction and work well for space-constrained locations.
A rotary vane-style compressor utilizes rotating vanes. Meanwhile, a reciprocating compressor operates more like an engine using pistons and cylinders to create compressed air. The cyclic motion of a reciprocating compressor creates more vibrations and noise but is known for its high-pressure gear. The rotary vane-style compressor machine also converts power to compressed air but utilizes cylinder rotors that minimize pulsations and vibrations with efficiency.
Here at Genemco, we offer the world's largest inventory of pre-owned industrial and manufacturing refrigeration equipment or gear. You can shop some of the most premium brands like Fuller, Frick, and FES without having to pay premium costs. Or you can even sell your own machine or tool. Start shopping for rotary vane compressors and compressor parts on our site. You can also contact an expert from our team regarding any questions.
Top Sellers
View all