Ammonia Diffusion Tanks
Diffusion Tanks are critical for your Ammonia refrigeration system and diffusion systems.
- FAQs
Ammonia diffusion tanks are essential components used in the field of refrigeration and air conditioning. The tank serves the purpose of storing and distributing ammonia gas. This type of gas is typically used as a refrigerant because of its cooling effect. The diffusion tank is designed to handle the unique properties of ammonia gas, and its pressure-relief valves are made of high-quality materials such as steel or aluminum. Overall, the tank's diffusion system consists of valves and pipes to control the flow of ammonia and ensure precise distribution.
Yes. In diffusion tanks, ammonia enters through vaporization and diffusion. The tank is meant to create a closed environment where the ammonia is stored. Liquid ammonia converts into gaseous form which enters the tank through an inlet. The ammonia absorption also involves a high-pressure container. The ability to convert liquid to gas in the diffusion process creates an environment suitable for the desired industrial processes.
- Before you can understand the function of an ammonia refrigeration system and its tanks, you'll want to learn the basics. For starters, ammonia is a colorless gas with a sharp, pungent odor. It's lighter than air and is necessary to maintain a healthy environment within the tank. Diffusion occurs when the pressure differences between two areas cause the gas molecule to move from one area of higher pressure to another area of lower pressure. Learn the step-by-step process here:
- First, the ammonia gas is compressed by a compressor, increasing its pressure and temperature. The high-pressure ammonia then flows into a condenser.
- The condenser will condense the ammonia refrigerant into a liquid. This liquid ammonia will then pass through an expansion valve and reduce its high pressure. The mixture enters an evaporator where it absorbs heat, causing the liquid to evaporate into a gas.
- Now, the diffusion process begins. The evaporated gas is finally at a lower temperature. It moves toward the suction line, which serves as a pathway for the gas to flow back to the compressor. This completes the refrigeration cycle.
Genemco is the best place to purchase pre-owned refrigeration equipment. In fact, we have the largest inventory of high-quality equipment for refrigeration systems. Shop for everything from surge drums and ammonia diffusion tanks to evaporative condensers and screw compressors. Feel free to contact our customer service team for any questions you may have regarding equipment for sale when it comes to your industrial refrigeration system. Our team has years of experience handling food processing and refrigeration machinery, so you can rest assured that we have what you need to optimize your manufacturing applications. Find the next solution for your facility here.
Top Sellers
View all