Votators & Scraped Surface Heat Exchangers
- FAQs
- ←
- →
Generally, a votator scraped surface heat exchanger is used for the sterilization and pasteurization of low-fat or low-viscosity emulsions that contain proteins and stabilizers, to avoid the spoiling of the emulsion, and as homogenizers. They're also used in ice cream, natural gas, and hydrogen production. They use a motor, so you'll need to determine how much horsepower you need. You can find many of the top votator II heat exchanger brands in our online store, including: Alfa Laval, APV, Chemetron, Creamery Package, Crepaco, and DeLaval.
The design of a scraped surface heat exchanger consists of a rotating shaft, agitator, paddles, and housing. The main benefit of using a scraped surface heat exchanger in a commercial refrigeration system is improved efficiency. That means your heat exchanger reduces the amount of energy required for the refrigeration system. The systems are typically used with liquid ammonia. Many of our exchangers are also mounted on frames on casters for convenience.
The primary benefit offered by shopping for used votators and scraped surface heat exchangers is the amount of money you can save, but there are others too. For example, by ordering pre owned equipment, you're shortening the amount of time you'll have to wait to receive your equipment. You can avoid the delays associated with buying new equipment. It's also the more environmentally responsible choice, as buying pre owned heat exchangers avoids reliance on the production of new equipment.
There's no doubt that your business, manufacturing company, or process plants could benefit from a votator scraped surface heat exchanger. We also sell a wide range of other commercial refrigeration equipment, including coolers, conveyors, refiners, transformers, compressors, freezers, evaporators, boilers, chillers, generators, and more. Our products aren't just available within the United States or North America, we offer many global shipping options as well. If you need something that cools your facility, then you're likely to find it at Genemco.
Top Sellers
View all