Compressors

Genemco offers top-of-the-line, used compressors for several industrial applications

We offer industrial compressors from Frick, FES, Vilter and other leading manufacturers.

Frequently Asked Questions

Industrial compressors are powerful machines used in a wide range of industries, including refrigeration. In the context of industrial refrigeration, air compressors play a crucial role in maintaining a stable and efficient cooling system. Industrial refrigeration systems consist of various components, such as rotary screw compressors, condensers, evaporators, and expansion valves. The primary function of an air compressor in this setup is to compress and circulate the refrigerant gas throughout the system. By compressing the refrigerant, the air compressor raises its pressure and temperature, converting it into a high-pressure gas.

This pressurized gas is then passed through the condenser, where it releases heat and cools down. The cooled refrigerant is then expanded through an expansion valve, causing it to vaporize and absorb heat from the surroundings, thus cooling the industrial space. Once the heat is absorbed, the cycle repeats as the refrigerant is compressed and circulated again by the air compressor. If you need optimal refrigeration and food processing, then you need high-performing, durable commercial air compressors for industrial applications.

One of the major advantages is that used equipment is readily available. While purchasing new equipment may involve waiting for production and shipping, used equipment is typically available immediately. This can be advantageous if you have an urgent need for the equipment or if you are looking to replace a faulty unit quickly. Pre-owned industrial compressors have also already undergone a break-in period. This means that any potential mechanical issues or faults have likely been identified by the previous owner. This provides peace of mind to buyers, as they can trust that the equipment has been thoroughly checked and is ready for use.

Additionally, since used equipment is often sourced from businesses that have upgraded or downsized, you can find a wide variety of options to choose from at a better price, allowing you to select the best fit for your specific needs. Moreover, opting for used compressors also contributes to sustainable and eco-friendly practices. By giving these compressors a second life, businesses reduce waste and promote a circular economy. It aligns with the growing emphasis on sustainability and responsible consumption, appealing to environmentally-conscious consumers and enhancing a company's reputation.

At Genemco, we have the world's largest inventory of pre-owned industrial refrigeration and food processing equipment. That means that whatever your needs are, we can meet them. With our 175,000 feet of warehouse space and 30 acres of inventory, we can shorten lead times by cutting out the middleman. You can expect to receive a high-quality, trustworthy commercial air compressor at a much faster speed than you would working with any other supplier. We ship globally and have thousands of clients who can tell you all about our commitment to customer satisfaction.

    With so many types of compressors out there, it can be difficult to choose which model is best for you. Fortunately, our wide range of compressors) offer plenty of options for many types of commercial and industrial businesses. Common types of compressors you can find at Genemco are:
  • Semi-Hermetic Compressors
  • Scroll Compressors
  • Rotary Vane Compressors
  • Gas Compressors
  • Split Rack Systems

    Some of the top brands you can find at Genemco include:

  • Carlyle
  • Carrier
  • Copeland
  • Frick
  • Fuller
  • Hill Refrigeration
  • Hitachi
  • Trane
  • Vilter
  • York
  • and more!

Carriers assist us in providing estimates for your delivery date, though you should always keep in mind that unexpected events like natural disasters can delay shipping. As previously mentioned, you will receive your order more quickly when you opt for pre-owned pieces of equipment. This can be valuable for businesses that need their refrigeration equipment quickly for commercial or industrial uses. We can provide more specific shipping information when you consult us about your needs.

Genemco ships internationally, so you can order your used compressors and have them delivered to numerous countries all over the globe. Our shipping rates are location-based, so when you work with us, we can provide you with an accurate quote based on the details of your order. To see if your country is eligible for shipping, you can check out our global shipping map. If you have any questions that weren't covered in this FAQ, please reach out to one of our experts so we can tell you more about our industrial compressors and other services.