- Water Supply: The process begins with a water supply system that provides water to the ice maker
- Freezing Plates: The heart of an industrial plate ice maker is the freezing plates. These plates are large, flat surfaces made of a highly conductive material, often aluminum
- Ice Production: Industrial plate ice makers leverage the principles of freezing water on large, cold plates. The water is spread evenly across the freezing plates, and as it freezes, a layer of ice forms on the plates. This process is repeated until a desired thickness of ice is achieved
- Harvesting and Storage: Once the ice has formed on the freezing plates, it is harvested and stored. The harvested ice is usually stored in a bin or silo until it is needed. Industrial plate ice makers are designed to produce ice continuously, ensuring a steady supply for various applications such as cooling, food processing, and more
- Advantages of Plate Ice: Plate ice has several advantages compared to other types of ice. It has an even cooling effect and a constant refrigeration temperature. It also melts more slowly, allowing for longer storage times compared to other types of ice

In summary, industrial plate ice makers differ from other ice makers in their design, focusing on the use of freezing plates to efficiently produce large quantities of ice. The resulting plate ice has unique characteristics that make it suitable for various industrial applications.
Visit Genemco.com for your next quality-used plate ice maker!