When it comes to industrial refrigeration equipment, there are many benefits to businesses purchasing used equipment, like used reciprocating compressors over new ones. Used equipment is often less expensive than new, and it can still provide the same level of performance and functionality. Another significant benefit of buying a used compressor is that it can help businesses reduce their environmental impact. Used equipment has already been manufactured and operated, so it doesn't require the same amount of resources to produce new equipment. This can be a big deal for businesses that are looking to reduce their carbon footprint. Purchasing used industrial refrigeration equipment is a chance to get high-quality equipment without breaking the bank. That's not all, a used compressor can save you a ton of time as well! This is because when you order a pre-owned piece of refrigeration equipment, it can be shipped immediately. That means you can get it up and running in your plant much faster than you would if you had to go through the process of buying a new compressor. If you're in the market for preowned reciprocating compressors, this article will teach you everything you need to know about buying used equipment.
What is a reciprocating compressor?
A reciprocating compressor is a positive displacement compressor in which the displacement is achieved through the action of a piston moving back and forth in a cylindrical chamber. The pistons compress the gases as they move up and down in the compressor cylinder. This type of compressor compresses air and other natural gas for use in applications such as air compressors, gas compressors, and refrigeration systems. Since new compressor equipment can be pricey, many businesses invest in used reciprocating compressors.
These compressors are used in refrigeration systems to compress and cycle refrigerant gas through the system. The refrigerant gas is compressed under high pressure and cooled as it flows through the condenser. The cooled refrigerant gas is then circulated through the evaporator, where it absorbs heat from the air resulting in cooled air. The refrigerant gas is then compressed again and returned to the condenser.
Reciprocating piston compressors have three main components: the compressor body, the compressor piston, and the compressor valves. The compressor body is the main structure of the compressor. It houses the compressor piston, the compressor valves, the bearings, and the seals. The compressor piston is a cylindrical piece in the compressor body. It's connected to the crankshaft, and the motion of the crankshaft causes the piston to move up and down. The compressor valves control the airflow in and out of the piston compressor.
There are several other compressor types, including rotary and screw-type compressors and centrifugal compressors. They function differently than piston compressors. The rotary screw compressor consists of a screw or a screw-shaped rotor that is rotated within a cylindrical housing. The rotor compresses the gas or fluid as it moves along the length of the screw. A rotating screw compressor is a device that increases a gas's or liquid's pressure. Another type of compressor is a centrifugal compressor. Centrifugal compressors are gas compressors that use a rotating impeller to pressurize gas. The impeller is a wheel-like structure that is surrounded by curved housing. As the impeller spins, it forces the gas to flow through the housing, increasing the gas's pressure.
How can your business use a reciprocating compressor?
Used reciprocating compressors are used extensively in industrial refrigeration systems. They are simple, reliable, and efficient machines that can handle a wide range of applications. Industrial refrigeration systems with reciprocating compressors are often used in businesses that require a large amount of cooling, such as hospitals, supermarkets, and data centers. They can also be found in companies with many cooling units, like restaurants and bars. The compressor can provide the necessary air pressure to run the equipment, helping to speed up the manufacturing process. In some cases, it may also be used to dry the product, helping to improve the quality and consistency of the final product.
Cylinder reciprocating compressors are a common type of compressor. They are used to compress gases and transfer energy to the gas. The compressor has a piston that moves inside a cylinder. Energy is transferred as the piston moves up and down. This gas is then compressed and transferred to another area.
There are many different uses for reciprocating compressors. Compressors can also be used in beverage and food processing and other applications. In addition, compressors can provide compressed air for cooling systems. If you are looking for a reliable piece of equipment that can be used for a variety of purposes, used reciprocating compressors from Genemco are the right choice for your business.
What do you need to consider when shopping for a used reciprocating compressor?
If you're shopping for a used compressor, there are a few factors you need to take into account when choosing one for your business. The most important factor is the compressor's power and capacity. Reciprocating compressors come in both oil-free and oil-lubricated versions. Oil-free compressors are less expensive and better for non-flammable fluids applications. Oil-lubricated compressors are more expensive but better for flammable fluids applications.
When considering the compressor's power, you need to examine the following factors:
Horsepower (HP): The horsepower rating of a compressor is the amount of power the compressor can produce. This rating is important to know because it helps you determine how powerful the compressor is. The more horsepower the compressor has, the more work it can do at once.
Capacity (CFM): CFM refers to the maximum amount of air a compressor can produce at a given pressure level measured as cubic feet per minute (CFM). The higher the CFM, the more air the compressor can produce. If you are looking for a compressor that can handle heavy-duty applications, you can find the perfect one for your industrial operations at Genemco.
Also, consider if you want a single-, two-, or three-stage compressor. Single-stage compressors are smaller and less expensive but have a lower compression ratio. This means they can't handle as much air as a two-stage compressor. If you need a compressor with a high compression ratio, you'll need to go with a two-stage or three-stage reciprocating compressor. The three-stage compressor has a variety of benefits over a single-stage compressor. The three chambers create a more consistent power output, meaning the compressor doesn’t have to work as hard to achieve the desired pressure. The three-stage compressor is better able to handle fluctuations in air pressure, meaning it can work in a broader range of applications.
Another factor in evaluating used reciprocating compressors is the inlet and outlet sizes. The inlet size is the size of the opening where the air enters the compressor, while the outlet size is the size of the opening where the compressed air leaves the compressor. Some compressors are also specifically designed to compress a certain type of gas or to be used to perform specific functions. When comparing different reciprocating compressors, consider how much air each can produce.
What else do you need to know about industrial reciprocating compressors?
The industrial reciprocating compressor has been in use for over a century and is still the most common type of compressor in use. There are several reasons for its popularity. Reciprocating compressors are relatively simple and rugged devices that are easy to maintain and operate. They also have a relatively low cost. The reciprocating compressor can compress gases at a wide range of pressures. This makes it a self-contained engine that does not require an external ignition source. A used reciprocating compressor can help your business in many ways, including:
- Reduced energy costs: A reciprocating compressor can help you save energy by controlling the compressor's speed to match the system's needs. It can also improve your production process and help you comply with environmental regulations.
- Increased production: A used compressor can help your production process because it can handle more pressure and produce more air than an outdated one. It increases output by providing a more consistent flow of compressed air.
- Improved quality: A used industrial compressor can help you produce a higher quality product by providing a more consistent airflow.
- Increased uptime: Used reciprocating compressors can help you increase uptime by providing a more reliable and consistent compressed air source.
Why does your business need a used industrial reciprocating compressor?

When businesses are looking for new equipment, the price is always a top concern. And for a good reason, buying new equipment can be a significant investment. But many businesses don’t realize that they can save money by opting for used industrial equipment instead. You can find high-end models with excellent capacity and even premium fan motors. A fan motor is responsible for blowing air through the compressor to keep it cool. This is a key part of the compressor because if it's not cooled, the compressor can overheat and be damaged.
Finding a quality used compressor is beneficial for your business. A better compressor will be more energy efficient, saving you money on your energy bills. It will also be more reliable, meaning you will spend less time and money repairing it. Another reason to find a used compressor you can trust is that it can help you improve your production. A durable and functional compressor can handle more work, allowing you to produce more products in a shorter amount of time. This can enable you to grow your business and keep up with your competition.
You're making a wise decision by choosing used industrial reciprocating compressors. Reciprocating compressors are some of the most reliable and durable compressors on the market. They can provide you with years of quality service, making them an excellent investment for your business. Additionally, a used or preowned compressor can be far more affordable than a brand-new model. When shopping for a used reciprocating compressor, consider the needs of your business. Make sure to choose a model that is the right size and has the features you need, and include the cost of repairs and maintenance in your calculations. Beyond just saving money on the base price of your equipment, your business can also save thousands of dollars by ordering equipment that is ready to ship from Genemco.
A used reciprocating compressor can be integral to your operations, but only if it's properly taken care of. Reciprocating compressors are easy to maintain and offer a high-reliability level. A preowned reciprocating compressor is an excellent option if you're looking for an affordable and reliable compressor. Find a reputable seller to ensure you get a quality product. Genemco is here to help if you're unsure where to look or how to get started. We have a wide selection of used reciprocating compressors and can help you find the perfect model for your business. We also offer a variety of services, including repairs and maintenance, so you can be sure your compressor will run smoothly for years to come.