Ammonia vs. Freon

 

Ammonia (NH₃) and Freon (a trademarked name for a group of fluorocarbon refrigerants, including CFCs, HCFCs, and HFCs) are two common types of refrigerants used in various cooling and refrigeration applications. Here are the key differences between them:

Chemical Composition and Properties:

  • Ammonia (NH₃):

    • Ammonia is a natural refrigerant composed of nitrogen and hydrogen.
    • It has a strong, pungent odor.
    • It is a highly efficient refrigerant with excellent thermodynamic properties.
    • Ammonia is toxic and can be harmful if inhaled in large quantities.
    • It is also flammable under certain conditions.
  • Freon:

    • Freon is a brand name for a variety of synthetic refrigerants, typically composed of fluorocarbons (CFCs, HCFCs, and HFCs).
    • Freons are generally odorless or have a faint, sweet smell.
    • They are less efficient than ammonia in terms of heat transfer properties.
    • Freons are generally non-toxic and non-flammable, making them safer to handle.
    • Many Freons have high Global Warming Potential (GWP) and some contribute to ozone depletion.

Environmental Impact:

  • Ammonia:

    • Ammonia has a negligible GWP and no ozone depletion potential (ODP).
    • It is considered environmentally friendly.
    • However, ammonia spills can be hazardous to health and the environment.
  • Freon:

    • Older Freons, such as CFCs and HCFCs, have significant ODP and contribute to the depletion of the ozone layer.
    • Many newer Freons (HFCs) have high GWP, contributing to global warming.
    • The use of many Freons is being phased out or regulated due to their environmental impact.

Applications:

  • Ammonia:

    • Commonly used in large industrial refrigeration systems, such as food processing plants, cold storage warehouses, and ice rinks.
    • Preferred for applications where high efficiency and low environmental impact are critical.
  • Freon:

    • Widely used in residential and commercial air conditioning systems, refrigerators, and small to medium-sized refrigeration systems.
    • Preferred in applications where safety and ease of handling are more important than environmental considerations.

Cost and Availability:

  • Ammonia:

    • Generally less expensive than many Freons.
    • Requires specialized equipment and handling due to its toxicity and flammability.
  • Freon:

    • Prices vary depending on the type of Freon and regulatory restrictions.
    • More widely available and easier to use in a variety of systems.

In summary, ammonia is highly efficient and environmentally friendly but requires careful handling due to its toxicity and flammability. Freon is safer to handle and widely used but can have significant environmental impacts, especially older types that harm the ozone layer and newer types with high GWP. Genemco carries and abundant amount of quality used equipment that uses ammonia as well as equipment that is equipped to use freon. Browse our extensive online inventory at Genemco.com.