Cost Savings Of Used Industrial Refrigeration Systems

 

The cost of industrial refrigeration systems and equipment can be quite expensive for businesses, but there is a great way to save money on these systems. Utilizing used industrial refrigeration is a great way to save money and still maintain efficiency and quality. Used industrial refrigeration systems and equipment offer many cost-saving benefits, including lower upfront costs and lower maintenance costs. In this blog, we will discuss the cost savings associated with using used industrial refrigeration systems and equipment.


The cost of new industrial refrigeration equipment can be quite expensive for businesses, but there is a great way to save money on these systems. Utilizing used equipment is a great way to save money and still maintain efficiency and quality.

Image from Genemco.com




When it comes to the cost of industrial refrigeration systems and equipment, the upfront costs are typically the highest expense. This is why it is important to consider the cost savings associated with using a used system. Used industrial refrigeration systems typically have a lower upfront cost than a new system. In addition, businesses can often find used systems that are still in good condition and offer the same features as a new system. Genemco is a great place to shop for used industrial refrigeration equipment. They have over 30 years of satisfied returning customers as well as a large inventory to choose from. In fact, they have the largest inventory of used industrial ammonia refrigeration equipment in the world! In addition, Genemco provides realistic negotiable quotes to customers, rather than the solid sticker price of new equipment. And if you need multiple items, you can bundle and save even more with Genemco.

Image from Genemco.com




Another cost saving associated with using a used industrial refrigeration system is that the cost of maintenance can actually be lower than maintenance on new equipment. A used system typically requires parts that can be easily found online or from a parts dealer, which can save businesses time and money. In addition, a used system can often be easier to repair than a new system.


Overall, selecting used industrial refrigeration equipment can save businesses an enormous amount of money. In addition to the cost savings mentioned above, businesses can also save money on installation costs. Another cost-saving perk when shopping with Genemco is that you can save even more money because all of their inventory is on-site, in stock, and ready to ship as soon as the next business day. That means you won't experience long lead times, which can be up to a year, like when purchasing new. By considering the cost savings associated with using a used system, businesses can ensure that they are getting the best value for their money.

Image from Genemco.com