Step into the cool world of coils! Through this article, you will learn the difference between low and medium temperature evaporator coils! The primary difference between low-temperature and medium-temperature evaporator coils lies in their operating conditions and intended applications.
Low-temperature evaporator coils are designed to operate at lower temperatures, typically below freezing. They are commonly used in applications such as commercial and industrial freezers or blast freezers. These coils are built to handle colder environments efficiently.
Image from Genemco.com:
On the other hand, medium-temperature evaporator coils are intended for applications where temperatures are higher, usually above freezing but not as extreme as in low-temperature cases. Examples include walk-in coolers, refrigerated display cases, or industrial food processing applications.
Image from Genemco.com:
The key distinctions are the materials used, design specifications, and refrigerant choices. Low-temperature coils need to withstand harsher conditions and might have additional features to prevent frost buildup, while medium-temperature coils focus on maintaining a more moderate temperature range.
To further explain, below is a breakdown of the comparison between low and medium temperature industrial evaporator coils:
-
Temperature Range:
- Low-Temperature Evaporator Coils: Designed for applications where the required temperature is below freezing (typically -20°F or lower). Examples include blast freezers and certain cold storage applications.
-
Medium-Temperature Evaporator Coils: Suited for applications where temperatures are above freezing but still relatively low (typically between 20°F to 35°F). Examples include walk-in coolers, food processing, and some cold storage applications.
-
Design and Construction:
- Low-Temperature Evaporator Coils: Constructed with materials and design features to withstand extremely low temperatures. This may include special coatings or materials to prevent frost build-up.
-
Medium-Temperature Evaporator Coils: Designed to operate at moderate temperatures and may not require the same level of insulation or anti-frost features.
-
Refrigerants:
- Low-Temperature Evaporator Coils: Selected to work efficiently with low-temperature refrigerants, such as those used in deep freezing applications.
-
Medium-Temperature Evaporator Coils: Compatible with refrigerants suitable for medium-temperature applications.
-
Heat Transfer Efficiency:
- Low-Temperature Evaporator Coils: Designed for efficient heat transfer at very low temperatures, considering the specific properties of the refrigerant used.
-
Medium-Temperature Evaporator Coils: Optimized for heat transfer at moderate temperatures.
-
Application Specifics:
-
Low-Temperature Evaporator Coils: Commonly found in industries such as industrial food processing, pharmaceuticals, and any application requiring deep freezing.
-
Medium-Temperature Evaporator Coils: Widely used in commercial refrigeration, supermarkets, and industries where milder cooling is sufficient as well as in some industrial applications.
-
Low-Temperature Evaporator Coils: Commonly found in industries such as industrial food processing, pharmaceuticals, and any application requiring deep freezing.
-
Energy Efficiency:
- Low-Temperature Evaporator Coils: May require more energy due to the lower temperatures involved.
-
Medium-Temperature Evaporator Coils: Tend to be more energy-efficient for applications with higher operating temperatures.
-
Frost Build-Up:
- Low-Temperature Evaporator Coils: Prone to frost accumulation, requiring defrosting mechanisms or special features to mitigate frost build-up.
- Medium-Temperature Evaporator Coils: Typically experience less frost accumulation, and some designs may not require defrosting.
Therefore, the choice between low-temperature and medium-temperature evaporator coils depends on the specific needs of the application, including the required temperature range, energy efficiency considerations, and the nature of the products being stored or processed. Each type of coil has its advantages and limitations, and selecting the right one is crucial for the overall performance and efficiency of the refrigeration system.
Shop for your next low or medium temperature evaporator coil from Genemco. Did you know that Genemco houses the largest inventory of used industrial refrigeration equipment in the world?
Image from Genemco.com: