The Process

The process of producing soy sauce on an industrial scale involves several steps to ensure quality and consistency in the final product. The first step is the preparation of the soybeans. In this process, the beans are cleaned and soaked in water to remove any impurities and soften them for further processing.
After soaking, the soybeans are cooked and then crushed to extract the liquid known as soy milk. The soy milk is then combined with roasted wheat to create a mixture, which is fermented using a type of mold called koji. This fermentation process usually takes several days and is essential for developing the distinct flavor and aroma of soy sauce.

Once fermentation is complete, the mixture is combined with brine, water, and a small amount of yeast to initiate a secondary fermentation process. This secondary fermentation further develops the flavor of the soy sauce. The mixture is then left to ferment for a specific period, which can range from a few months to several years, depending on the desired flavor and quality.
Throughout the production process, specialized equipment is used. This includes large vats or barrels for fermentation, as well as grinding and mixing machines. Additionally, temperature-controlled rooms or even underground cellars are often used to maintain optimal conditions for fermentation.
After the fermentation process is complete, the soy sauce is filtered and pasteurized to remove any impurities. It is then packaged in bottles, jars, or containers, depending on the manufacturer's preference. The packaging is typically designed to protect the soy sauce from light and air, which could deteriorate its quality.

To ensure the soy sauce reaches stores in good condition, it is usually shipped in large containers or drums. These containers are sealed to prevent leakage or spoilage during transportation. Once the soy sauce reaches its destination, it is then unpacked and distributed to retailers for sale to consumers.
Overall, the process of producing soy sauce on an industrial scale involves various steps, including soybean preparation, fermentation, filtering, pasteurization, packaging, and shipping. The use of specialized equipment and controlled environments ensures consistent quality and flavor in the final product.