The Process

Firstly, producing beef jerky on an industrial level involves several steps to ensure the meat is safely processed and flavorful. The beef is sourced and inspected for quality and freshness. Once approved, it is then sliced into thin strips. These strips are marinated in a mixture of spices and flavorings to enhance the taste and tenderize the meat.
After marination, the strips are transferred to industrial-grade dehydrators or smokehouses. These specialized types of equipment ensure the meat is slowly dried at low temperatures or smoked to perfection. This drying process removes the moisture from the meat, extending its shelf life and giving it the desired chewy texture.
Once the correct moisture level is achieved, the beef jerky is cooled and inspected again for quality control. It is then ready to be packaged and shipped to stores. The packaging of beef jerky is typically done using airtight plastic pouches with zip locks to maintain freshness and prevent spoilage. These pouches are often vacuum-sealed to further extend the product's shelf life.
During the packaging process, labels are applied to identify the flavor, nutritional information, and any other relevant details. Additionally, some manufacturers may choose to include oxygen absorbers or moisture control packets in the packaging to maintain the quality of the beef jerky.

After packaging, the beef jerky is carefully boxed and prepared for shipment. It is either distributed directly to retailers or sent to distribution centers, where it will be further distributed to various stores. The shipping process involves careful handling and temperature control to ensure the beef jerky reaches stores in optimal condition for consumption.
In summary, the production of beef jerky on an industrial level involves sourcing and inspecting the beef, marinating and drying the meat using specialized equipment, packaging it in airtight pouches, and shipping it to stores for distribution. This process ensures that consumers can enjoy high-quality beef jerky that is flavorful, tender, and safe to consume.