How Industrial Mini Tube Ice is Created

Industrial mini-tube ice makers are machines designed to produce small cylindrical ice tubes commonly used in various applications, including food and beverage service, healthcare, and scientific research. These ice makers operate on a basic principle of freezing water into tubes, which are then harvested and stored for later use. Here's a step-by-step explanation of how they work:

Image Source: Genemco



  1. Water Supply: The ice maker is connected to a water source, usually a potable water supply. It's essential that the water source is clean and free from impurities to ensure the quality of the ice produced.

  2. Water Filtration: In some systems, the water may pass through a filtration system to remove any sediment, minerals, or impurities. Clean water helps produce clear and tasteless ice.

  3. Ice Mold or Evaporator: Inside the ice maker, there is a specialized component called an evaporator or ice mold. This mold is typically made of food-grade stainless steel and is designed to freeze water into ice tubes. The mold has rows of cylindrical cavities where the ice tubes will form.

  4. Water Distribution: A water distribution system is responsible for filling the cavities in the ice mold with water. It usually includes pumps and pipes that evenly distribute water over the mold's surface.

  5. Refrigeration System: The heart of the ice maker is its refrigeration system. It consists of a compressor, condenser, and evaporator coils. This system works together to lower the temperature inside the ice maker.

  6. Freezing Process: The water flows over or into the ice mold cavities. As it comes into contact with the cold evaporator coils, it begins to freeze. The refrigeration system keeps the temperature sufficiently low to ensure that the water freezes slowly and evenly, forming cylindrical ice tubes.

  7. Harvesting: Once the ice tubes have reached the desired size and consistency, the ice maker initiates the harvesting process. This is often done by using hot gas or a heating element to release the ice from the mold. The ice tubes are then separated from the mold and fall into a storage bin or container below.

  8. Storage Bin: The ice falls into a storage bin where it is collected until it's needed. The storage bin or cold storage room usually has insulation to keep the ice from melting too quickly.

  9. Controls: The ice maker is controlled by a computerized system that monitors the ice-making process, including water levels, ice formation, and temperature. It also initiates the harvest cycle when the ice is ready.

  10. Distribution: Users can access the ice from the storage bin as needed. Some systems have mechanisms to dispense ice automatically into containers or machines, such as ice dispensers in a restaurant or healthcare setting.

  11. Cleaning and Maintenance: Regular cleaning and maintenance are essential to ensure the ice maker's continued performance and hygiene. This includes sanitizing the ice-making components, changing filters, and inspecting the system for any issues.

Industrial mini-tube ice makers are designed for efficiency and reliability, making them a crucial component in various industries where a consistent and clean ice supply is required.