The pharmaceutical and biotechnology industries rely heavily on precise temperature and humidity control to maintain product integrity, ensure safe production environments, and meet stringent regulatory standards. Industrial evaporator coils are a critical component in achieving these environmental controls by providing cooling, dehumidification, and refrigeration in various applications. Below are the key ways in which industrial evaporator coils are used within these industries:
Image from Genemco
Link to Industrial Evaporator Coils
1. Cold Chain Logistics
Pharmaceuticals and biologics, such as vaccines, hormones, and enzymes, are often temperature-sensitive and must be kept within strict temperature ranges to preserve their efficacy and safety. Industrial evaporator coils are vital in cold chain logistics, which involves the transportation and storage of these products under controlled conditions from the point of manufacture to the end user.
- Refrigerated storage: Evaporator coils are used in cold storage facilities to maintain low temperatures for pharmaceuticals and biological materials. These cooling systems ensure that products are stored in the appropriate environment to prevent degradation.
- Vaccine storage: Vaccines are highly sensitive to temperature changes and require storage at specific temperatures to remain effective. Cold storage systems with evaporator coils ensure consistent cooling, keeping vaccines stable during storage and distribution.
- Refrigerated transport: Evaporator coils are also employed in refrigeration units for trucks and containers used in the transport of pharmaceuticals and biological products, maintaining the required temperatures during shipping and distribution.
2. Cleanroom Environments
Pharmaceutical and biotechnology production processes often take place in cleanrooms where air quality, temperature, and humidity are tightly controlled to prevent contamination and ensure product quality. Industrial evaporator coils are used in HVAC systems to help maintain the controlled environment necessary for sterile manufacturing.
- Temperature control: Evaporator coils regulate the temperature inside cleanrooms, ensuring the environment remains within the specified range. This is particularly important for temperature-sensitive processes like drug formulation, mixing, and filling.
- Humidity control: In addition to temperature regulation, evaporator coils are used to control humidity levels, preventing the growth of bacteria, mold, or other contaminants that could compromise the sterile environment. Controlling humidity also helps prevent degradation of hygroscopic materials, which absorb moisture from the air.
3. Pharmaceutical Manufacturing Facilities
In pharmaceutical manufacturing plants, temperature regulation is critical at various stages of production to ensure product consistency, safety, and quality. Industrial evaporator coils are used in HVAC and refrigeration systems to provide the necessary cooling during these processes.
- Drug formulation: Many pharmaceutical ingredients are sensitive to temperature changes, and evaporator coils help maintain controlled temperatures during drug formulation and mixing. By cooling the air or the process materials, these coils ensure the ingredients remain stable and effective.
- Lyophilization (freeze-drying): Freeze-drying is a process used to preserve pharmaceuticals, particularly vaccines, proteins, and other biological materials. Industrial evaporator coils play a key role in lyophilization by providing the cooling necessary to freeze the product before the sublimation of water occurs, transforming the product into a dry, stable form.
- Tableting and capsule filling: During the tableting and capsule filling process, excessive heat can affect the integrity of the drug compounds. Evaporator coils in the facility’s HVAC system help manage the heat generated during these processes, ensuring product stability.
4. Biotechnology Research and Development
In biotechnology research and development (R&D) labs, temperature-sensitive biological processes, such as cell culture, protein synthesis, and genetic engineering, require precise environmental control. Industrial evaporator coils are used to regulate the temperature and humidity in these lab environments, which is crucial for the success of the experiments.
- Incubation chambers: Evaporator coils are used in incubators that maintain optimal temperatures for the growth of bacteria, yeast, and mammalian cells. These systems ensure the accuracy of experimental results and the viability of cell cultures.
- Bioreactors: Bioreactors, which are used to grow microorganisms or cells in controlled conditions, often require precise temperature control. Industrial evaporator coils cool the air or liquid in these systems, allowing researchers to maintain the optimal temperature for biological reactions.
- Freezers and cryogenic storage: Biotechnology labs often use ultra-low temperature freezers and cryogenic storage for the preservation of biological samples, such as DNA, RNA, and cell lines. Industrial evaporator coils help maintain the extreme cold temperatures required for long-term preservation.
5. Sterile Storage Facilities
Pharmaceutical products, especially injectable drugs and biologics, are often stored in sterile environments that require temperature control to prevent contamination and degradation. Industrial evaporator coils help regulate these conditions in sterile storage facilities, ensuring that products remain stable and ready for distribution.
- Storage of injectable drugs: Injectable drugs, including vaccines and insulin, are highly sensitive to temperature and require storage in refrigerated environments. Evaporator coils in cold storage systems ensure the drugs are kept within the specified temperature range to maintain their potency and safety.
- Blood and tissue storage: Blood products, tissues, and organs for transplantation require strict temperature control to preserve their viability. Industrial evaporator coils are used in blood banks and tissue storage facilities to provide the necessary refrigeration for these life-saving materials.

6. Environmental Chambers for Stability Testing
Pharmaceutical companies are required to conduct stability testing to ensure that their products maintain efficacy and safety throughout their shelf life. This involves storing drugs under various environmental conditions, such as different temperatures and humidity levels, and testing their stability over time. Industrial evaporator coils are used in environmental chambers to create the necessary conditions for this testing.
- Stability testing chambers: Evaporator coils are used to maintain specific temperatures and humidity levels in stability chambers where pharmaceutical products are stored for extended periods. These chambers simulate different storage conditions, such as extreme heat or cold, to determine how the products will react over time.
- Shelf-life studies: By providing consistent cooling and humidity control, evaporator coils in environmental chambers help pharmaceutical companies conduct reliable shelf-life studies, which are required by regulatory bodies like the FDA.
7. Pilot Plants for Drug Development
In pilot plants, where new drugs are developed and tested on a smaller scale before full production, industrial evaporator coils are used in cooling systems to regulate the temperature during the manufacturing of trial batches. These facilities often require precise temperature control to ensure the success of early-stage production.
- Cooling during drug formulation: Evaporator coils provide cooling during the formulation of trial drug batches, ensuring that the ingredients remain stable and the production process is consistent with large-scale manufacturing standards.
-
Temperature-sensitive process control: In pilot plants, some processes, such as crystallization or chemical reactions, require specific temperatures for the drug compounds to develop correctly. Evaporator coils help maintain the necessary temperatures, contributing to the success of these processes.
In the pharmaceutical and biotechnology industries, industrial evaporator coils play an indispensable role in maintaining the environmental conditions required for drug production, storage, and distribution. From cold chain logistics to research labs and manufacturing facilities, evaporator coils ensure that temperature and humidity are precisely controlled to protect sensitive materials, ensure product efficacy, and comply with regulatory standards. As the industry continues to advance with new therapies and technologies, the demand for efficient and reliable evaporator coil systems will only grow, driving innovation in cooling technologies across these sectors.