One word...Shaq!! You may know the backboard shattering, 7-foot-1-inch, 325-pound Shaquille O'Neal from his long-standing professional NBA career. Or, if you were a 90's kid you may know him as the genie from Kazaam. Maybe you know him from his business savvy investments in companies like Google, Vitaminwater, Lyft, Ring, and several restaurant franchises. Either way, there is one thing we all know about Shaq, he has a large appetite for the biggest and the best! Whether that's business opportunities, appearances, or an insatiable appetite..... he wants more! And his recent partnership with Meat District gives us exactly that.
Announced on National Cheeseburger Day, Shaquille O'Neal introduced The Shaq Burger! According to Refrigerated Frozen Foods and Meat District "The Shaq" features Angus beef brisket, chuck, and short rib mix blended in just the right proportions so each burger is perfectly tender, flavorful, and juicy. This is a pure unadulterated burger made from the absolute best meat cuts. The bottom line is it’s the best-tasting burger you’ve ever had, period.
Sounds delicious but how does "The Shaq" measure up to a standard patty from the refrigerated section at the local grocer? Let's start with the size. The typical burger patty is about 1/3 lb. and usually consists of one type of meat. The Shaq patties are 1/2 lb. each and consist of brisket, chuck and short rib! I guess the only thing short about Shaq is the short rib in his patties... and maybe a free throw or two.
Feeling inspired and hungry create your own meaty eats? Consider these products from Genemco to help make your delicious dream come true...
Mixer/Grinder
Contact Plate Freezer.
Remember to keep your grinder and meat cold and to run the meat through the grinder twice! For other great tips and tricks check out No Spoon Necessary.
Image and information credit to Meat District