In the agriculture industry, industrial evaporator coils are critical components in climate control and refrigeration systems that help maintain optimal conditions for crop storage, livestock environments, and greenhouse operations. Effective temperature and humidity management is essential to preserving the quality of produce, improving agricultural yields, and ensuring the welfare of livestock. Industrial evaporator coils are used in cooling, drying, and refrigeration systems that support these objectives.
Image from Genemco
Link to Evaporator Coils
Here’s an in-depth look at how industrial evaporator coils are applied in various agricultural processes:
1. Post-Harvest Storage and Preservation
One of the most important uses of industrial evaporator coils in agriculture is in post-harvest storage systems, where crops, fruits, vegetables, and other perishable products need to be kept at specific temperatures and humidity levels to prevent spoilage and maintain freshness.
Cold Storage Facilities
- Refrigeration of perishable goods: After harvesting, fruits and vegetables must be stored in cold environments to slow down their metabolic processes and extend their shelf life. Industrial evaporator coils in refrigeration systems are used to lower the temperature in cold storage facilities, maintaining the freshness of products such as apples, lettuce, berries, and other temperature-sensitive items.
- Moisture control: Humidity control is also important in cold storage. Too much moisture can lead to mold growth, while too little can cause produce to dry out. Evaporator coils are essential in dehumidification systems that balance humidity levels, ensuring that stored produce retains the proper moisture content.
Controlled Atmosphere Storage (CA)
- Extended shelf life of crops: Controlled atmosphere storage is a method used to extend the storage life of fruits and vegetables by controlling oxygen, carbon dioxide, and nitrogen levels along with temperature and humidity. Industrial evaporator coils are used in these systems to maintain precise temperature control, reducing the respiration rate of stored products like apples, pears, and other high-value crops. This process helps slow ripening and decay, allowing produce to be stored for extended periods without compromising quality.
Grain and Seed Storage
- Grain drying and cooling: After harvesting, grains and seeds need to be dried to prevent spoilage caused by moisture. Industrial evaporator coils in air conditioning or dehumidification systems are used to cool and dry grains in silos or storage facilities. By removing excess moisture and controlling temperature, evaporator coils help reduce the risk of mold growth, insect infestation, and spoilage, preserving the quality of stored grains.
- Maintaining seed viability: Seeds used for planting in subsequent growing seasons must be stored in controlled environments to maintain their viability. Evaporator coils help create the ideal conditions for seed storage by regulating temperature and humidity levels, ensuring that the seeds remain healthy and ready for planting.
2. Greenhouse Climate Control
Greenhouses are used to grow crops in controlled environments where temperature, humidity, and light conditions can be managed to optimize plant growth and yield. Industrial evaporator coils are integral to greenhouse climate control systems, where they are used for cooling, dehumidification, and air circulation.
Temperature Control in Greenhouses
- Cooling systems: In hot climates or during the summer months, greenhouse temperatures can become too high for plants to thrive. Evaporator coils are used in cooling systems to lower the temperature inside the greenhouse, preventing heat stress in plants. This is particularly important for delicate crops like flowers, leafy greens, and herbs, which require stable temperatures to grow optimally.
- Energy-efficient cooling: Industrial evaporator coils also contribute to energy-efficient climate control in large-scale greenhouse operations. By efficiently removing excess heat from the air, these coils help reduce energy consumption and operational costs, allowing growers to maintain the ideal conditions for plant growth without excessive energy use.

Humidity Control for Optimal Plant Growth
- Dehumidification in humid climates: Excess humidity in greenhouses can lead to mold growth, fungal diseases, and other issues that negatively impact plant health. Evaporator coils in dehumidification systems help remove excess moisture from the air, keeping humidity levels within an optimal range for plant growth. This prevents the development of diseases like powdery mildew and ensures better yields.
- Maintaining moisture balance: Some crops, such as tomatoes and cucumbers, require specific humidity levels to grow effectively. Industrial evaporator coils help manage this by removing or adding moisture to the air as needed, ensuring that plants receive the right environment for robust growth.
3. Livestock and Poultry Farming
The welfare and productivity of livestock and poultry are closely tied to the environmental conditions in which they are housed. Industrial evaporator coils are used in climate control systems for barns, poultry houses, and other animal housing facilities to regulate temperature and air quality, improving animal health and production efficiency.
Temperature Control in Livestock Housing
- Cooling systems for livestock: Heat stress can negatively affect livestock, reducing productivity, and in severe cases, leading to illness or death. Evaporator coils are used in cooling systems that lower the temperature inside barns or animal housing facilities, ensuring that livestock such as cattle, pigs, and chickens are kept in comfortable conditions. These systems are particularly important in hot climates or during the summer months, where high temperatures can cause heat-related stress in animals.
- Energy-efficient ventilation: Evaporator coils are also part of energy-efficient ventilation systems that help circulate cool air throughout animal housing facilities. By maintaining proper air circulation and cooling, these systems help prevent respiratory problems and improve overall animal welfare.
Improving Air Quality in Poultry Houses
- Controlling humidity and ammonia levels: In poultry farming, high humidity and ammonia levels from manure can lead to respiratory issues in chickens and reduce overall flock productivity. Evaporator coils in ventilation and dehumidification systems help remove excess moisture and maintain optimal air quality in poultry houses. This not only improves the health and growth rates of the birds but also reduces the risk of diseases spreading through the flock.
- Temperature and humidity control for brooding: Young chicks are particularly sensitive to environmental conditions. Evaporator coils in climate control systems are used to maintain the precise temperatures and humidity levels needed for successful brooding, ensuring higher survival rates and better early development.
Image from Genemco
Link to Evaporator Coils
4. Agricultural Processing and Cold Chain Logistics
Agriculture also involves processing products into market-ready goods, which requires careful temperature management during handling, processing, and transportation. Industrial evaporator coils play an essential role in agricultural processing facilities and cold chain logistics, ensuring that perishable products maintain their quality from farm to market.
Cooling in Processing Plants
- Fruit and vegetable processing: Many agricultural products are processed immediately after harvesting to maintain freshness. Industrial evaporator coils are used in cooling systems in processing plants to quickly lower the temperature of produce, preventing spoilage and maintaining quality during processing. For example, evaporator coils are used in cooling tunnels for produce like berries and leafy greens, ensuring rapid cooling after harvest and before packaging.
- Meat and dairy processing: In meat and dairy processing facilities, maintaining low temperatures is critical to preventing bacterial growth and ensuring product safety. Evaporator coils in refrigeration systems are used to cool carcasses, milk, and other animal products during processing, helping preserve product quality and extend shelf life.
Cold Chain Logistics
- Refrigerated transportation: Evaporator coils are used in refrigerated trucks and containers to keep agricultural products at optimal temperatures during transport. This is especially important for perishable goods like fruits, vegetables, meat, and dairy products, which must be transported through a cold chain to avoid spoilage. The cooling provided by evaporator coils ensures that products remain fresh and safe for consumption when they reach the market.
-
Maintaining product integrity: Cold chain logistics is crucial for products that require consistent temperature control, such as fresh produce and frozen goods. Industrial evaporator coils are integral to refrigeration systems that maintain these conditions throughout transport, helping to prevent spoilage, reduce waste, and ensure food safety.
Industrial evaporator coils are essential in the agriculture industry, playing a key role in post-harvest storage, greenhouse climate control, livestock housing, and cold chain logistics. By providing efficient cooling, humidity control, and air circulation, evaporator coils help preserve the quality of crops, improve animal welfare, and ensure that perishable products are safely transported from farm to market. Through their application in agricultural systems, evaporator coils contribute to enhancing productivity, reducing waste, and improving overall efficiency in farming operations.