Image from Genemco
Link to industrial evaporator coils

1. Textile Industry
The textile industry involves the processing of natural and synthetic fibers to create fabrics, which often requires precise control over the temperature and moisture content of the production environment. Industrial evaporator coils are essential in achieving this, helping to maintain ideal conditions in spinning, weaving, dyeing, and finishing processes.
Spinning and Weaving Processes
- Temperature and humidity control: Textile fibers, especially natural fibers like cotton and wool, are sensitive to changes in temperature and humidity. If the air is too dry or too humid, fibers can break or stretch, leading to defects in the fabric. Evaporator coils are used in air conditioning and dehumidification systems to maintain optimal conditions for spinning and weaving. By cooling and controlling the air, evaporator coils ensure the fibers maintain the right amount of moisture, reducing breakage and improving the quality of the final product.
- Static electricity control: In synthetic fiber production, static electricity can build up if the air is too dry, causing fibers to stick together and leading to production issues. Evaporator coils help control the humidity levels, reducing static buildup and ensuring smooth operation of weaving machines.
Dyeing and Finishing
- Cooling dyeing equipment: Dyeing textiles often involves the use of heated water or steam to fix the dyes into the fabric. After the dyeing process, evaporator coils are used to cool down the water or air used in the system, ensuring the fabric is properly rinsed and finished at the correct temperature.
- Controlling moisture during finishing: During finishing processes like calendering (smoothing the fabric), moisture levels in the air must be carefully controlled to avoid fabric shrinkage or stretching. Evaporator coils are used in HVAC systems to dehumidify the air, keeping the environment at the right moisture levels and ensuring the fabric retains its desired properties.

Air Conditioning and Ventilation in Production Facilities
- Worker comfort and safety: Textile factories often have high heat loads due to the operation of machines, such as spinning frames and looms. Evaporator coils are used in air conditioning systems to cool the production floor, improving the working environment for employees and reducing the risk of heat stress.
-
Improved equipment performance: In addition to worker comfort, cooling systems that use evaporator coils help protect sensitive textile equipment from overheating, ensuring machines can operate continuously and efficiently.
2. Paper Industry
The paper industry involves a series of complex processes to convert raw materials, such as wood pulp, into paper products. Throughout this process, controlling the temperature and moisture levels is critical for achieving high-quality paper and maintaining the efficiency of machinery. Industrial evaporator coils are used in various stages of paper production to regulate conditions and enhance productivity.
Pulping and Papermaking
- Moisture control in drying sections: After the wood pulp has been processed into a slurry, it is spread onto screens and passed through dryers to remove excess moisture. Evaporator coils are used in dehumidification systems to remove moisture from the air in the drying section, ensuring that the paper dries uniformly and without defects. Proper humidity control helps avoid issues like paper warping or curling, which can occur if the drying process is uneven.
- Heat recovery and cooling: The papermaking process generates a lot of heat, particularly during the drying and pressing phases. Evaporator coils are part of heat recovery systems that transfer excess heat from the process to cooler air or water, reducing energy consumption and preventing equipment overheating. These systems help maintain a stable production environment while optimizing energy use.
Coating and Calendering
- Cooling of coated paper: After the paper has been formed, some products require coatings to enhance properties like gloss, texture, or water resistance. These coatings are applied at high temperatures, and evaporator coils are used in cooling systems to cool the paper and the coating equipment, ensuring the paper can be handled and further processed without damaging the coating.
- Maintaining ideal conditions for calendering: In the calendering stage, where paper is smoothed and compressed between rollers, controlling the temperature and humidity is essential to achieving the desired finish. Evaporator coils in HVAC systems help regulate these conditions, preventing the paper from becoming too dry or brittle as it passes through the rollers.
Environmental Control in Paper Mills
- HVAC systems for paper storage: Finished paper products must be stored in controlled environments to maintain their quality and prevent issues like curling or wrinkling due to humidity changes. Industrial evaporator coils are used in air conditioning and dehumidification systems within storage areas to ensure that the paper is kept at a consistent moisture level.
- Worker comfort and safety: Similar to the textile industry, paper mills generate significant heat during production, particularly in the drying and coating stages. Evaporator coils are used in air conditioning systems to cool down production areas, creating a safer and more comfortable working environment for employees. These systems also prevent the overheating of machinery, reducing downtime and maintenance costs.
Cooling of Machinery
-
Cooling paper-making machines: Paper machines, such as Fourdrinier machines, which form the paper from pulp, generate a lot of heat during operation. Evaporator coils are used in the cooling systems of these machines to prevent them from overheating and to ensure the efficient production of paper. By cooling the circulating air or water, the evaporator coils help maintain stable temperatures, reducing equipment wear and tear.
- Cooling of hydraulic systems: In both the textile and paper industries, hydraulic systems are often used to operate heavy machinery. Evaporator coils are essential for cooling the hydraulic fluids in these systems, ensuring that the machinery operates efficiently and that the fluids maintain their viscosity, which is critical for proper functioning.
Industrial evaporator coils are integral to the operation of both the textile and paper industries, where the control of temperature and humidity is essential to the production process. In the textile industry, evaporator coils help regulate the environment for spinning, weaving, dyeing, and finishing operations, ensuring high-quality fabric and minimizing fiber damage. In the paper industry, these coils are vital for managing moisture during the pulping, drying, and coating processes, ensuring that the final product meets quality standards and equipment runs efficiently. By optimizing environmental control and cooling machinery, industrial evaporator coils play a key role in enhancing productivity, reducing energy consumption, and ensuring the longevity of equipment in both industries.