Evaporative Condenser Explained

 

If you're a left-brainer, this article is for you! We know evaporative condensers are important in our industry but how do they work exactly? Here is a breakdown to answer that question. Plus, we've included visual diagrams for all of us right-brainers too!

An evaporative condenser is used to remove excess heat with the cooling effect of evaporation from a cooling system to improve the heat rejection process when the heat cannot be utilized for other purposes.
Water is sprayed over the condensing coil from above while air is simultaneously blown up through the coil from below to naturally lower the condensing temperature. Then the refrigerant goes to an expansion valve which changes from high pressure to low pressure and makes the refrigerant very cold. Next, the cold refrigerant goes to the evaporator. (evaporative coil, ice maker barrel, etc.) 


Image Credit: BAC, Evapco.








Genemco is a pre-owned industrial refrigeration and food processing equipment dealer and is the largest pre-owned ammonia refrigeration reseller in the world. 
We carry a large variety of evaporative condenser brands and sizes. Some of our most popular brands include Evapco, BAC, and Imeco.


Our refrigeration category includes these subcategories: 
Ice Freezers & Chillers 
Compressors 
Evaporator Coils 
Condensers & Cooling Towers 
Recirculators, Receivers, Vessels 
Chillers & Coolers 
Other Refrigeration

Our other categories of products we carry include:
Evaporators & Boilers 
HTST & Heat Exchangers
Pumps, Homogenizers & Tanks
Motors & Electrical 
Fillers, Conveyors & Packaging 

 

 

3385 S. San Gabriel St. Hearne, TX 77859
Phone: (979) 268-7447

Email: sales@genemco.com



Source Credit 
Source Credit 
Source Credit