It's a "cool' world in the refrigeration industry, especially when it comes to ice, its varieties, and how it's made on an industrial scale! Industrial flake ice makers are fascinating devices. They essentially produce small, flat, and thin pieces of ice, resembling flakes. Here's a simplified breakdown:
-
Water Supply: The process begins with a water supply. This water is usually filtered to ensure purity and then pumped into the ice maker.
-
Water Distribution: The water is evenly distributed over the surface of a rotating drum or a cylindrical evaporator. This drum is kept extremely cold, usually below the freezing point of water.
-
Freezing Process: As the water flows over the drum, it freezes into a thin layer. The rotating motion of the drum prevents the ice from sticking and ensures an even thickness.
-
Ice Removal: A blade or a mechanism is used to scrape the thin layer of ice off the drum's surface. The result is a continuous flow of small, flat ice flakes.
-
Collection and Storage: The collected ice flakes are then stored in a bin or transported for immediate use. Some systems may include additional steps for drying or separating excess water from the ice.
-
Temperature Control: The entire process is carefully controlled to maintain the right temperature and ensure efficient ice production. This involves a refrigeration system to keep the drum cold.
-
Automation: Many industrial ice makers are automated, with sensors and controls to monitor the ice-making process. This helps in maintaining optimal conditions and adjusting production based on demand.
Industrial flake ice has a range of applications, from food processing and preservation to concrete cooling in construction. It's valued for its ability to quickly cool and mold around objects. Check out Genemco.com for all types of industrial ice makes and refrigeration equipment.