Evaporators

Genemco offers used Evaporators from top manufacturers

Shop popular brands like APV, SPX, and Goulds.

Concentrator Plates
Recently Sold
Concentrator Plates
Sold outRecently Sold

Evaporators are used to evaporate liquid into a gaseous state via heat transfer. All evaporators have mechanisms to separate liquid and vapor by means of a heat transfer. The raw material passes through heated tubes and evaporates the water within the material. Evaporators consist of a container, or vessel, into which liquid is added. The liquid is then exposed to a heating medium and vaporized at boiling point, usually by a heat exchanger or steam. As the liquid evaporates, the vapors are collected in the vessel. The vapors can go through a condenser and be turned back into a liquid concentrate or used as a gas, depending on the application.

Used evaporators are utilized to turn liquid chemicals into vapor. This piece of equipment can be used in a variety of applications, including food production, pharmaceutical manufacturing, chemical plants, and more. In the food industry, evaporators are used to reduce the water content of juice, syrup, and other liquids to concentrate their flavor and texture. In the pharmaceutical industry, evaporators are used to reduce the moisture content of medicines and other pharmaceuticals. This helps improve the stability of the product and prevent it from degrading over time. In the chemical industry, evaporators are used to separate components of a mixture, such as oils and solvents. This is done by heating the mixture and allowing the more volatile components to evaporate, leaving behind the less volatile components. Turning liquid chemicals into vapor is known as distillation.

Evaporators are designed to handle a wide range of evaporation with a heating medium. Some evaporators allow 99 percent evaporation in a single pass, while others require multiple distillation passes to achieve the same results. Evaporators can be used to reduce the concentration of a solution, remove impurities, or recover solids from a solution. The most common types of evaporators are falling film evaporators, rising film evaporators, forced circulation evaporators, plate evaporators, batch evaporators, and mechanical vapor recompression evaporators.

No matter if you're in the food industry or another area, buying used evaporators is a great way to save money when you're looking to expand your refrigeration system or need to replace an existing evaporator. Used equipment can be a cost-effective solution compared to buying a brand-new unit. Buying used equipment is also a great way to help the environment, as it reduces waste and increases sustainability. If you're looking for an efficient and cost-effective way to add or replace an evaporator in your refrigeration system, then considering a used evaporator is a great option.