Screw Compressor Motors
- FAQs
- ←
- →
Choosing the right compressor motor for a particular job is a decision that requires careful consideration. You can start by deciding whether you want a dry screw compressor on an oil-flooded compressor. Oil-flooded compressors, as the name would suggest, utilize compressor oil as a lubricant to function, while dry compressors use the principle of positive displacement and air pressure to provide power. You need to select a motor that's rated to provide enough horsepower output for the compressor. Some of the brands in our online store include A.C. Squirrel, Baldor, Toshiba, GE, Ram Industries, SIEMENS, Teco, and more!
Make sure you understand the details of the standard compressor parts, including the rotors, valves, pumps, coolers, transducers, and gauges, so you can be informed as a consumer. Rotary screw compressors use two intermeshed screws. The screws are the main component of the compressor, and the air system is driven by an electric motor. Rotary screw air compressors are designed to provide a steady and reliable flow of air or gas by utilizing a variable speed drive (VSD).
- There are three primary reasons why you should think about buying a preowned rotary screw compressor engine for your business.
- Cost: By looking for used screw compressor motors, you can save without sacrificing quality or performance.
- Efficiency: You can reduce waste and make efficient choices by shopping pre-owned.
- Speed: You won't have to wait or put up with the delays that are often associated with purchasing new equipment.
Beyond purchasing your compressor, you can find other industrial refrigeration accessories at Genemco too, including condensers, evaporators, generators, and other types of refrigeration equipment. When you shop with us, you can trust that all parts of the machine, from silencers to thermal valves to oil coolers, will be in good working order. There's no doubt that if you're in need of high-quality compressor motors, then your best bet is to shop at Genemco.