Rotary Screw Compressor Packages

Genemco offers Full Rotary Screw Compressor Packages

Shop popular brands like GEA, FES, Vilter and Frick

FES Ammonia Twin-Screw CompressorFES Ammonia Twin-Screw Compressor
Sold out
Frick Screw Ammonia CompressorFrick Screw Ammonia Compressor
Sold out
Frick Screw Ammonia CompressorFrick Screw Ammonia Compressor
Sold out
Frick Screw Ammonia CompressorFrick Screw Ammonia Compressor
Sold out
Frick Screw Ammonia CompressorFrick Screw Ammonia Compressor
Sold out
Frick RXF 39 Screw CompressorFrick RXF 39 Screw Compressor
Sold out
Mycom 200 Rotary Screw Compressor Package - 75 HPMycom 200 Rotary Screw Compressor Package - 75 HP
Sold out Recently Sold
Mycom 200 Rotary Screw Compressor Package - 75 HPMycom 200 Rotary Screw Compressor Package - 75 HP
Sold out Recently Sold
Frick RWF 480 Compressor RotorsFrick RWF 480 Compressor Rotors
Sold out Liquidation

Screw compressors are an essential component of industrial refrigeration systems, playing a role in the overall cooling process. Unlike reciprocating compressors that use pistons to compress and move refrigerant gases, screw compressors utilize two interlocking rotating helical rotors to achieve compression. During the compression process, the rotation of the rotors draws in the refrigerant gas from the intake port.

As the gas enters the expanding chambers, it becomes trapped and is subsequently compressed as the chambers reduce in volume. The pressure and compressing action created by the rotating screws increases the pressure and temperature of the refrigerant. The compressed air and refrigerant gas is then discharged from the screw compressor and sent to the condenser, where it undergoes a heat exchange process to dissipate the accumulated heat. The now-cooled refrigerant continues its journey through the system, ready to repeat the cooling cycle to maintain the desired pressure and temperatures in an industrial setting.

Many parts play a role in making a compressor function. For example, the oil separator plays a crucial role in the operation of a rotary screw compressor. Its primary function is to separate the oil from the pressure-compressed air, ensuring that only clean, oil-free air is delivered to the end-use application. This is particularly important in industries such as manufacturing, automotive, and food processing, where the quality of the compressed air can directly impact the final product.

There are many types of screw compressor packages, from bare screw compressors to piston or rotary vane compressors. Each type has its own set of advantages, making it suitable for specific applications. Understanding the different types of screw compressors can help businesses make informed decisions when selecting the most suitable compressor.

As any refrigeration industry veteran can tell you, purchasing a rotary screw compressor package from Genemco should be your top choice when you need new refrigeration equipment. First of all, Genemco offers a wide range of rotary screw compressors that are designed to meet the unique requirements of various industries. These packages come in different sizes and capacities, allowing you to find the perfect fit for your specific needs.

Beyond that, our rotary screw compressor packages from Genemco are renowned for their exceptional quality and reliability. We source their compressors from top brands, so you can trust that you will receive a product that is built to last. These compressors are known for their durability, with robust construction and high-quality components (the motor drive, valve, turbine, radiator, tank, separator, pump, air filter, propeller, electric motor, engine, etc.) that are designed to withstand the demanding conditions of industrial or commercial applications.

You can always expect excellent customer service and support as well. Our team of experts is dedicated to helping you choose the right compressor package for your needs and providing any assistance you may require.

    Generally, the reputation and history of a brand can play a major role in establishing consumer trust. We know that your business needs the best equipment at an affordable price and at Genemco, you can find high-end equipment from industry leaders. Some of the top compressor brands you can find at Genemco include:
  • Copeland
  • Dunham-Bush
  • FES
  • Frick
  • GEA
  • Howden
  • Mycom
  • Reco
  • Sullair
  • Trane
  • Vilter
  • and more!

    You can reach out to us if there is a specific brand or product you're looking for. We have a wide range of options available and we can point you in the right direction with a little more information about your needs. We also offer other types of refrigeration products, so you can locate everything from a reciprocating compressor to an evaporator to a heat pump or heat exchanger.

While buying a brand-new compressor may seem like the obvious choice, the truth is there are many more advantages to buying a used or pre-owned piece of equipment. Cost savings are a major advantage of purchasing a pre-owned rotary screw compressor. This allows you to allocate your budget towards other business needs. This is especially beneficial for small and medium-sized businesses that may be operating on a limited budget.

Additionally, buying used equipment means avoiding the enormous depreciation hit that new equipment experiences as soon as it’s purchased. This can be a big relief to business owners who want to ensure they get the most out of their investment. Furthermore, purchasing pre-owned screw compressor packages from a reputable seller like Genemco can still provide you with a machine that's in fantastic condition.

Using a pre-owned compressor can give you a more energy-efficient tool that will allow you to continue to meet your volume and production quotas while protecting your products and promoting safety. Many used compressors are still in great shape and have a long service life ahead. Reputable sellers often refurbish and thoroughly inspect their pre-owned compressors, ensuring that they're in optimal working condition before being sold. This gives you peace of mind knowing you're investing in a reliable piece of equipment that will meet your business's air compression needs.

All of the inventory you see on our website is in stock, ready to ship, and owned outright! We partner with the most reliable shipping companies to ensure hassle-free and timely delivery. If you want to know what shipping will cost, reach out to us today! We can give you a quote based on your particular location.

You can reference our global shipping map, which offers more information on where we can ship our products outside of the United States. As you'll see, there are many countries we can ship to, particularly in Central and South America. When you place your order, we will put together a shipping quote for you based on the location where you would like your screw compressor packages delivered.